Drive systems for measuring and testing technology

Unrivaled measuring performance.

maxon drives work reliably in many fields of measuring technology. From high-precision measurements in the semiconductor and surface technology industries to construction site and landscape surveying in rainy, snowy and cold conditions - we find an ideal solution for every measuring application.

Technologie

Weltweit führende Antriebstechnik.

Absolut exakte Messungen durch automatische Prüfgeräte werden für die Wissenschaft, das Bauwesen, aber beispielsweise auch für die Qualitätssicherung in der Industrie immer wichtiger. maxon Antriebe übernehmen weltweit bei vielen Marktführer wichtige Funktionen in der Messtechnik.  

Präzision

Hohe Lebensdauer

Geringe Baugrösse

Hohe Leistungsdichte

Energieeffizienz

Zuverlässigkeit

Technologie

Auf den Mikrometer genau.

In der Mess- und Prüftechnik müssen Antriebe Bewegungen häufig auf den Mikrometer genau ausführen. Außerdem müssen Messgeräte heute in der Lage sein, lange Reihe von Tests automatisch und reproduzierbar durchzuführen. maxon Motoren mit Positioniersteuerungen übernehmen diese Aufgaben absolut zuverlässig in: 

3D-Messmaschinen

LiDAR-Systemen

Oberflächenprüfgeräten

Scanner

Total Stationen

Präzisionswaagen

Robert Höll

General & Technical Manager

Qness

“The drives from maxon need to be very precise. After all, they need to move the slide with micrometer precision. We cannot afford any compromises here. Our accuracy is now far superior to that required by the standard.”

Corporate Blog

Success stories

Drive solutions from maxon meet the high requirements of measuring and testing technology for accuracy, precise motion sequences, and reproducibility in numerous applications.
Go to the blog
Versatrax 100 Pipe Inspection Crawlermaxon Story

These robots crawl into every nook and cranny

It started as a project by two engineers who were close to retirement. Today, the modular inspection robots by Canadian company Inuktun are successfully in use all over the world – defying even the most adverse conditions.
Learn more
1_ipek_supervisionmaxon Story

Pipe inspection with top power density.

Imagine the drain is clogged and not a single drop is flowing down any more. A common problem – the cause can be hidden in the far corners of a sewage system. This is where inspection robots come into play to hunt for the cause. Motors by maxon motor provide the robotic vehicles with a precision drive, among others uses. 
Learn more
Egripment_photo_Olympics_2_1800x1200maxon Story

Full power at the Olympics.

The Olympics 2020 took place in Tokyo, Japan in 2021 where 10,500 well-trained athletes from 204 different countries gathered and battled for the most wanted medals in 33 different kinds of sports. It is the time when we sympathize with these warriors and watch them perform with close attention through our television screens.
Learn more
Go to the blog

Contact

What challenges are you facing?

Our measuring and testing technology experts will be happy to help you.